Stamp Graphics

Stamp Graphics provide designers the ability to add graphics and notes to their designs. These are non-network graphics that are typically used to add details and explanatory notes to the final print or design.

Stamp Graphics are created and configured in ArcGIS Pro, and they are saved together as a .stylx file. Then, that .stylx file is uploaded in Solution Center > Designer > Client Application > Stamp Graphics. Once uploaded, designers have access to the entire collection of graphics included in the .stylx file.

You can have one .stylx file for Electric, and a different .stylx file for Gas.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?