Download a Snapshot

After a snapshot is created, you can download it.

IMPORTANT: This is helpful to transfer snapshots to other machines or servers. However, currently there is no customer-facing interface to upload a previously-downloaded snapshot. Your Schneider Electric implementation specialist can assist you if you need to upload a previously-download snapshot.

To download a snapshot, follow these steps:

  1. Along the left-hand side of the interface, click a snapshot once to highlight it in green. Then, view its details on the right-hand side.

    TIP: Use the Search along the top of the interface to search for a snapshot by its Title.
  2. At the bottom of the interface, click Download.

    IMPORTANT: There is no progress bar displayed, but after a short period of time your local Downloads folder automatically opens when the download is complete.
  3. Notice in your local Downloads folder, the application creates a folder using the GUID of the snapshot as the folder name. Further, it includes all the Assets that were part of the snapshot.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?