Add Global IDs

You can add Global IDs on all datasets to be used in ArcFM Mobile by using ArcCatalog or a Python script.

Use one of these methods to add Global IDs:

  1. To do this using a Python script, refer to Esri’s Add Global IDs article for further details.
  2. To do this using ArcCatalog, right-click on your dataset and select Manage > Add Global IDs. Given that this part of adding Global IDs takes a few minutes, you are prompted to acknowledge you want to continue.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.