Configure Markups for Operational Maps

The Markup subtab provides a list of markup types (defined on the Markup Types tab) that are available for the selected operational map. You can configure each markup type to use the default markup palette, or you can override those settings.


  • For each markup type in the list, leave the Use Default Palette toggle enabled if you want to use the default markup palette.


  • To completely disable the associated markup type on the selected map, toggle Use Default Palette off, then toggle Disable on.


  • To override the setting on the Markup Types tab for the selected markup type, toggle Use Default Palette off then provide a URL to the feature service that defines the markup palette for this type.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.