Outbound Message Integrations

ArcFM Mobile can make calls to external applications, and send selected assets and locations to other applications on mobile devices using URI scheme messages, These outbound messages allow you to activate external apps and pass them the attributes of a selected feature. External apps can be off-the-shelf products, such as ArcGIS Survey123, or custom apps and websites.

Configuring outbound messages is highly technical, so we created an entirely separate ArcFM Mobile Developer Guide for your reference.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.