Map Requirements

  1. To create replicas for individual regions, a polygon feature class is used. It can be included in a feature service with other point and polyline features, or it can be in a map service on its own and based on a different data set, such as landbase.
  2. Ensure your geometric network maps are valid. Esri’s Verify and repair geometric network connectivity tool helps verify your geometric network.
  3. Remove all annotation feature classes, which are not supported on feature services by Esri at this time.
  4. Remove all joins from feature classes, including ArcFM Feeder Manager 2.0 joins.
  5. In ArcFM, under Layer Properties > Fields, ensure that all the fields you want to view are visible, or the feature service absolutely won't recognize them.
  6. Any field that is a unique identifier (such as GlobalID) or is a foreign key in a relationship must be visible.
  7. For cases in which multiple layers point to the same source feature class, each of these layers must have a unique name, and they must not be shown at the same zoom scale. Otherwise, ArcFM Mobile in offline mode cannot distinguish the data that corresponds with each layer.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.