Publish the Markup Feature Service

Follow Esri’s instructions for Publishing a map service. In place of Step 7, however, perform the following steps:

  1. Click Capabilities.
  2. Select the Feature Access checkbox.
  3. Click Feature Access on the left.
  4. Under Operations allowed, select Create, Delete, Query, and Update.

Proceed with Step 8 of Esri’s instructions.

Before markup capabilities are available to your users, you next must tell the application which feature service(s) to use. This is accomplished in Solution Center along with the remainder of markup configuration. Your next step is to Configure Markup Types.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.