Download Offline Packages

Downloading offline packages and having them readily available are the keys to getting the most out of ArcFM Mobile. Offline packages are designed by your system administrator and can be set up to contain different pieces of information, for example:

  • Just gas data

  • Just electric data

  • Both electric and gas data

  • Gas data for a particular region

  • Electric data for a particular region

  • Both electric and gas data for a particular region, etc.

If your administrator has configured your organization to use only offline data, you might see the following dialog the first time you launch the app after installing:

Click or tap the link to download an offline package.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.