Version All Tables

Follow the steps below to version all feature and object tables as required.

IMPORTANT: Tables that are part of the Utility Network (UN) get versioned automatically when you version the database connection. You need to manually manage and version any non-UN tables.

  1. In the Catalog pane, right-click the database connection and select Geodatabase Connection Properties.
  2. Set the Versioning type to Branch. Doing so sets all feature classes and tables that are in the UN.
For any tables that are not part of the UN (relationship classes, etc.) perform the following steps:
  1. Right-click each table name and select Manage.

  2. On the Manage pane, select the Versioning checkbox and the Branch radio button.

  3. Click OK.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.