View Markup Layers

Upon logging in to Markup tools, markup layers should appear in your map. However, if your organization uses a Portal for ArcGIS-federated server for markup, you have to first log in to Portal. Follow these steps:

  1. Connect to the desired ArcGIS Server.

  2. If your organization uses OAuth2 for Portal authentication, you must log in to the portal via File > Sign In. Specify a user that has permissions to the federated markup map service. If you aren’t certain if the user has the required permissions, check with your system administrator.

  3. If you’re already logged in to the Markup tools, then add the Markup Feature Service to the map.

NOTE: If your Markup Feature Service is ArcGIS for Portal-federated, refer to Esri’s Manage portal connections from ArcGIS Pro article for help ensuring that ArcGIS Pro is connected to the correct feature service.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.