SE-Managed Markup Service (Option 1)

A Schneider Electric-managed Markup Service deployment involves the installation and configuration of Microsoft Azure’s Hybrid Connection Manager. Each Hybrid Connection defines a specific on-premise HTTP endpoint to which ArcFM services can connect. ArcFM Markup services use these connections to write markups to ArcGIS Server. These endpoints can reside in a DMZ or other network segment, so long as they are accessible from the on-premise Microsoft HCM service.

HCM is configured in Solution Center. Refer to the Hybrid Connections topic in the Solution Center Configuration Guide for more information.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.