Publish a Feature Service

You need to follow Esri’s Publishing a map service steps, then in place of Step 6, perform the following:

  1. Click Capabilities.
  2. Select the Feature Access checkbox.
  3. Click Feature Access on the left.
  4. Under Operations allowed, check Query.

    NOTE:
    • At minimum, Feature Access and Query have to be selected since every map you publish must have those capabilities enabled whether or not you want them offline. If you ever intend on taking maps offline, Sync has to be enabled as well. If you select Sync, you should review the Offline Viewer Config section.

    • Feature Access with the Query operation must be enabled in your map service to allow querying of the map service to display features in the ArcFM Mobile app.

    • When offline, the Sync operation allows syncing of data when changes are made in the database.

IMPORTANT: For ArcFM Mobile users to have access to a feature service through Portal for ArcGIS for online and offline viewing, the feature service must either be shared with everyone or with groups where the users are members.

Proceed with Step 7 of the ArcGIS Resources instructions.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.