Add Operational Maps

After you’ve successfully added the feature service to one or more tenant groups, the remaining task is to add/configure operational maps.

The steps to add operational maps in ArcGIS Pro do not differ from the steps in ArcMap. Refer to the Add Operational Maps in the ArcMap section above.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.