Assign/Unassign/Complete

The Assign To Me, Unassign, or Complete buttons can be used to change the status of markups. Logged-in users can assign markups to themselves that are either unassigned or assigned to another user. You must have a markup selected in the Markup pane to complete any of these tasks below.

To assign a Markup to yourself, click the Assign To Me button.

To reassign a markup that is currently assigned to someone else, click the Assign To Me button. After a moment, the markup is reassigned.

Once assigned, a markup can be unassigned if it should be returned to the pool of available markups. To do so, click the Unassign button. You cannot unassign markups that are not currently assigned to you.

The markup can also be completed by clicking the Complete button.

Select Yes to complete the markup.

If you select No, the markup remains assigned. If you select Yes, the following things happen:

  • The markup is removed from the list.

  • The markup features are removed from the map and the app.

  • A notification is sent to the app that markups have been closed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.