Markups Pane

To display the Markups pane, click the Markups button. Be aware that only active markups are displayed. Each markup record displays its current status, who submitted the markup, the date it was submitted, and a number of operational choices. In the Markup pane, you can filter markups based on your assigned work, all available work, markup type, and markup name. You can also assign, unassign, or complete a markup. For viewing specific markups on the map, there is functionality that allows you to zoom to a particular markup and show just that markup in the map.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.