Offline Data Preparation

Add Global IDs on all relationship classes to be used in ArcFM Mobile by using Esri's Migrate relationship class tool. If your relationships are currently maintained via a user-managed field rather than an Esri-managed field, you don't need to migrate your relationship classes to use Global IDs.

If any changes are made to either a feature service that is used for a replica or to the structure of the geodatabase schema, you must delete and recreate all replicas for operational maps based on the feature service.

NOTE: Offline operational maps have some limits on layer symbology, and some advanced symbology supported in online maps is not supported in offline maps.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.