Configure Layer Settings

Depending on the version of ArcMap you have installed, layer settings may not be displayed in ArcMap the same as they are in Mobile. If ArcMap layers don't display as expected, follow the instructions in the topics in this section to correct the settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.