GPS for External Navigation Apps

ArcFM Mobile does not provide turn-by-turn navigation but instead integrates with third-party navigation apps for this capability. On Windows devices, many such apps, including Windows Maps and Google Maps, obtain position information only from Windows Location Services. They do not recognize external NMEA receivers unless the position data from these receivers is available through Location Services. Therefore, the NMEA receiver configuration in ArcFM Mobile does not eliminate the need for GPS position information in Location Services when integrating with some navigation apps.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.