Markup Palette Configuration

A markup tool palette is a toolbar full of markup elements that users can select to place in the view of an operational map. Palettes are available for users with Redlining license or higher. A palette is configured by creating a markup dataset in ArcMap (or ArcGIS Pro) and publishing a Markup Feature Service.

The instructions in this section walk you through configuring markup datasets that define the markup palette your users access. You can create as many markup palettes that make sense for your organization.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.