Feature Service Publishing

Read through and follow Esri’s instructions for Publishing a map service. In place of Step 7, however, perform the following:

  1. Click Capabilities.

  2. Select the Feature Access checkbox.

  3. Click Feature Access on the left.

  4. Under Operations allowed, select only Query and Sync. All other choices should remain unchecked.

Proceed with Step 8 of Esri’s instructions.

Feature Access must be enabled in your map service to allow querying of features, replica creation, and syncing of data in ArcFM Mobile when changes are made in the database.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.