Electric Domain
Electric Settings
|
Electric General Settings |
Settings |
|---|---|
|
ElectricDistributionTierName |
Electric Distribution |
|
TransformerAttachRadiusInMapUnits |
Enter a value, likely between 0.20 and 50.00. A structure found within this radius (with rules that allow attachment) is automatically considered as attached to the given device when performing an in-line network feature or transformer move. |
|
TransformerToLineRadiusInMapUnits |
Enter a value, likely between 0.20 and 50.00. This value is the default offset distance from the connection point and transformer during a transformer move. |
Electric Field Names
The Field Model Names listed below are displayed in Solution Center, and they are then pointed to user-selected database fields. For instructions on how to set field model names, refer to Configure Field and Class Model Names.
The Database Field Name column in the table below matches Schneider Electric sample data, however, it is not required that your data match these exactly. The database field names can be called anything you desire. However, it is required that the Field Model Names match as indicated in the table below.
Where there are more than one feature class listed in the table below, this implies that each feature class should have a database field name mapped to the field model name displayed. For example, in the first row in the table below, both ElectricLine and ElectricEdgeObject feature classes must contain a database field name for the conductor material that is mapped to the field model name, ConductorMaterial.
|
Field Model Name |
Feature Class |
Database Field Name |
Data Type |
Description |
|---|---|---|---|---|
|
ConductorMaterial |
ElectricLine ElectricEdgeObject |
conductormaterial |
Short |
Integer code for conductor material. |
|
ConductorOperatingVoltage |
ElectricLine ElectricEdgeObject |
voltagegroup |
Short or Long |
Integer code for the nominal operating voltage (values should include units and indicate whether the value is line-to-line or line-to-neutral). Examples:
|
|
ConductorSize |
ElectricLine ElectricEdgeObject |
conductorsize |
Short |
Integer code for conductor size. |
|
CustomerLoad |
ElectricSubnetline |
customerLoad |
Short or Long |
Designates a numeric field whose value is assigned by a subnetwork summary function that computes the sum of service panel amp ratings for all service points on the subnetwork. Used by Network Management in Editor XI to produce an estimate of feeder load MVA. |
|
DeviceStatus |
ElectricDevice ElectricJunctionObject |
devicestatus |
Short |
Values: Open, Closed |
|
ElectricSubnetworkName |
ElectricLine ElectricDevice ElectricEdgeObject ElectricJunctionObject |
subnetworkname |
Text |
Field to which the UpdateSubnetwork function writes the subnetwork name for a feature. |
|
FacilityId |
ElectricLine ElectricDevice ElectricEdgeObject ElectricJunctionObject |
assetId |
Text |
Identifier preferred by the organization implementing ArcFM. |
|
FuseRatedAmps |
ElectricDevice ElectricJunctionObject |
devicesize |
Short or Long |
Integer code for the fuse rating. |
|
IsGangOperated |
ElectricDevice ElectricJunctionObject |
gangoperated |
Short |
Indicates if the device controls all phases together. |
|
PhasesNetworkAttribute |
ElectricLine ElectricDevice ElectricEdgeObject ElectricJunctionObject |
phasesnormal |
N/A — network attribute, not a field. |
An in-line network attribute associated with the PhasesNormal field. |
|
PhasesNormal |
ElectricLine ElectricDevice ElectricEdgeObject ElectricJunctionObject |
phasesnormal |
Short |
Represents the phases present for each device. |
|
RatedKva |
ElectricDevice ElectricJunctionObject |
devicesize |
Short or Long |
Integer code for the power rating of a device (e.g. transformer rated power). |
|
StructureFacilityId |
Structure Boundary Structure Line Structure Junction |
assetId |
Text |
Identifier preferred by the organization implementing ArcFM, for structural facilities. |
Electric Field Names Interpretation Tab
-
Click on the Electric Field Names tab.
-
Click on the Interpretation tab on the right side.
-
Select the appropriate domain value in the following drop-down lists:
-
For the FilterValue meaning Closed: drop-down, select the domain value that sets a device to Closed.
-
In the FilterValue meaning Open drop-down, select the domain value that sets a device to Open.
-
Select which domain value you want other values to be assumed as in the All other values to be interpreted as drop-down.
-
-
Click Save to apply your settings.
Network Categories
In Editor XI, the concept of electric class model names used within a geometric network has been replaced with network categories used within a utility network.
A network category is a way to group features with similar characteristics that play a similar role within the network such as lines, devices, and junctions. These network categories help define behavior, tracing logic, and visualization within the utility network. The ArcFM UN data model differentiates network categories into two groups: equipment type categories and modeling categories. The equipment type categories are defined by the types of equipment these feature classes, asset groups, and asset types represent. Modeling categories are defined by the roles or functions they serve in the network.
A good example of an equipment type network category is E:Switch, which should be placed on all switchable device asset groups/asset types in the network. A good example of a modeling category would be E:Protective. This network category would be appropriate to assign to a device that can function as a protective device. One might assign this network category in order to run a protective trace to identify devices that can de-energize a section of the electrical network.
Some network categories may be subsets of others. A feature type that belongs to a E:Reclosing category, for example, should also belong to the E:Switch category. Other network categories are mutually exclusive. A feature type cannot belong to both the E:Transformer - Inline category and the E:Transformer - Tap category.
To learn more about the ArcFM UN data model and its required network categories, see the ArcFM UN Network Categories topic. To learn more about how to assign network categories, read the Esri help topic, Set or modify a network category assignment.
Assign the following network categories as described in each topic.
The following table displays the required network categories for the ArcFM XI series application, and in some cases, the specific tool.
ArcFM Editor XI
| Network Category | Application | Tool |
|---|---|---|
|
E:Conductor |
Editor |
None |
|
E:Conductor Info |
Editor |
|
|
E:Connection - Tap |
Editor |
|
|
E:Has Conductor Info |
Editor |
|
|
E:Has Connected Units |
Editor |
|
|
E:Has Disconnected Units |
Editor |
|
|
E:Service Point – Primary E: Service Point – Secondary E: Service Point – Critical |
Editor |
|
|
E:Protective |
Editor |
|
|
Subnetwork Controller |
Editor |
|
|
E:Switch |
Editor |
|
|
E:Switch - Fuse |
Editor |
|
|
E:Transformer |
Editor |
|
|
E:Transformer - Inline |
Editor |
|
|
E:Transformer - Tap |
Editor |
|
|
E:Unit |
Editor |
|
ArcFM Conduit Manager
| Network Category | Application | Tool |
|---|---|---|
|
E:Conductor Node |
Conduit Manager |
|
|
S:Duct |
Conduit Manager |
|
|
S:Duct Bank |
Conduit Manager |
|
|
S:Duct Bank End |
Conduit Manager |
|
|
S:Duct Bank Hub |
Conduit Manager |
|
|
S:Duct End |
Conduit Manager |
|
|
S:Duct End Flag |
Conduit Manager |
|
|
S:Duct Flag Direction Line |
Conduit Manager |
|
|
S:Duct Flag Leader Line |
Conduit Manager |
|
|
S:Duct Flag Outline |
Conduit Manager |
|
|
E:Conduit Occupant - Nonspatial Conductor |
Conduit Manager |
|
|
E:Conduit Occupant - Spatial Conductor |
Conduit Manager |
|
|
S:Vault |
Conduit Manager |
|
Autoupdaters
| Autoupdater Name | Required Network Categories | Details |
|---|---|---|
|
Auto Angle Setter |
None |
N/A |
|
Auto Structure Relate |
None |
Optionally, any category can be used for feature exclusion. To learn more, refer to the Auto Structure Relate topic. |
|
DXI Integration - Create Vertex or Junction |
None |
N/A |
|
Set Bank PhasesNormal and DeviceStatus |
|
Without the required categories, this autoupdater executes without failure, but may not make all intended edits. The PhasesNormal and DeviceStatus of a Device (i.e. Bank) is only set if it has the category E:Has Connected Units, while only contained Junction Objects (i.e. units) with the category E:Unit are used in calculations. To learn more, refer to the Set Bank PhasesNormal and DeviceStatus autoupdater topic. |
|
Update Length |
None |
N/A |
|
Update Line Terminal Connections |
None |
N/A |
|
Update Rated kVA |
|
Without the required categories, this autoupdater executes without failure, but may not make all intended edits. The Rated kVA (DeviceSize) of a Device (i.e. Bank) is only set if it has both categories: E:Has Connected Units, and E:Transformer, while only contained Junction Objects (i.e. units) with the category E:Unit are used in calculations. To learn more, refer to the Update Rated kVA autoupdater topic. |