Install the ArcFM Connectivity Evaluator (ACE) Tool
The ArcFM Connectivity Evaluator (ACE) is a separate application from Editor XI and Solution Center. Its core function is to test and verify connectivity to ArcFM services and, depending on the application, connectivity to Azure Service Bus. This is a crucial prerequisite before performing Solution Center configuration or any plugin configuration, as you need connectivity for the configuration to work.
When using the ACE tool, keep the following in mind:
-
Because the ACE tool is testing connectivity, it only works after your company’s tenant is created.
-
The ACE tool can be run as many times as needed until all issues are corrected. This is particularly helpful throughout the implementation process.
-
The ACE installer can be downloaded on the myArcFM page ArcFM Solution Center.
-
Install and run the ACE tool on the same machine that runs the XI application you are testing. In other words, if you are testing connectivity for Editor XI, run the tool on the same machine where Editor XI is installed.