Gas Traces

In this topic, we list the hard coded parameters that define our traces. See the Trace Results Options topic in the Editor Using Guide for information on user configurable settings for your trace.

Isolation Trace

This trace makes use of Esri’s Isolation tracer.

We use the following parameters:

  • Retrieve the GasDistributionTierName from the Gas Domain configuration

  • Functions are set to an empty list

  • Do NOT Validate Consistency

  • Include isolated features

  • Barriers are set to Regulator and Isolating devices

  • Filter results to show only meters, pipes, and open valves


We filter our trace results to show meters, pipes, and open valves in order to illuminate which valves should be closed to isolate a portion of the gas network.


System Trace

This trace uses Esri’s Connected Trace.

We use the following parameters:

  • Retrieve the GasDistributionTierName from the Gas Domain configuration

  • Functions are set to an empty list

  • Target tier and Source tier are null

  • Do NOT Validate Consistency

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.