Gas Domain

Gas Settings

Gas General Settings

Settings

GasDistributionTierName

Pipe Distribution System

PipeDiameterUnits

Centimeters

Gas Field Names

The Field Model Names listed below are displayed in Solution Center, and they are then pointed to user-selected database fields. For instructions on how to set field model names, refer to Configure Field and Class Model Names.

The Database Field Name column in the table below matches Schneider Electric sample data, however, it is not required that your data match these exactly. The database field names can be called anything you desire. However it is required that the Field Model Names match as indicated in the table below.

TIP: If your organization chooses to name your database fields differently than those listed in the column below, it is recommended that you record what database names you assigned to which field model names in place of the suggested names in the table. This list of differences will help assist Schneider Electric Support in the event you need their assistance with your database in the future.

Field Model Name

Database Field Name

DeviceAssetTypeNetworkAttribute

G_DEVICEASSETTYPE

DeviceCritical

importance

This field model name must be mapped to the text field which contains information about the operating classification of the valve (e.g. Critical). It is represented by Critical in Component Info.

IMPORTANT: While Component Info indicates Yes or No, the User Interface is searching for the string ‘cr’ in upper or lower case within the attribute of the valve feature. To denote that a valve is not critical do not use any words with ‘cr.’

DeviceDiameter

diameter

This field model name must be mapped to the field with proper domains related to the diameter of features in the map and is represented by Diameter in Component Info.

TIP: Changing the units in the Editor XI Configuration does not change the units of the diameter field.

DeviceMaterial

material

This field model name must be mapped to the field with proper domains related to the type of material the device feature is made from (e.g. Cast Iron, Steel) and is represented by Material in Component Info.

DeviceStatus

devicestatus

DeviceType

designtype

This field model name must be mapped to the field with proper domains related to the type of valve (e.g. Ball, Butterfly) and is represented by Valve Type in Component Info.

FacilityId

assetid

Field in which the title of the Component Info pane will show after a device is selected, e.g. ASSETID.

Pinchable

pinchable

PipeDiameter

nominaldiameter

StructureFacilityId

assetid

Gas Field Names Interpretation Tab

  1. Click on the Gas Field Names tab.

  2. Click on the Interpretation tab on the right side.

    Gas Field Names Interpretation tab

  3. Select the appropriate domain value in the following drop-down lists:

    • For the FilterValue meaning Closed: drop-down, select the domain value that sets a device to Closed.

    • In the FilterValue meaning Open drop-down, select the domain value that sets a device to Open.

    • Select which domain value you want other values to be assumed as in the All other values to be interpreted as drop-down.

  4. Click Save to apply your settings.

IMPORTANT: If the coded values in the drop-downs aren’t what you expected to see, check the DeviceStatus field mapping on the Fields tab.

Gas Field Names tab

Gas Class Model Names

Class Model Names don't have to match exactly as illustrated in the table below. You can set any of your features with the Gas Device model name as long it is a Controllable Device within Component Info.

Feature Class

Asset Group

Asset Type

Gas Device

Controllable Tee

Controllable Tee

Gas Device

Controllable Valve

System

Gas Device

Regulator

Regulator

Gas Device

Controllable Valve

Emergency

Gas Device

Meter

Custody Transfer

These model names are applied directly to a selection of asset types, or to all asset groups.

Model Name

Assign To:

GasValve

Assign this model name to valve asset types to enable Component Info functionality for the asset.

Network Categories

A network category is a way to group features with similar characteristics that play a similar role within the network such as lines, devices, and junctions. These network categories help define behavior, tracing logic, and visualization within the utility network. The ArcFM UN data model differentiates network categories into two groups: equipment type categories and modeling categories. The equipment type categories are defined by the types of equipment these feature classes, asset groups, and asset types represent. Modeling categories are defined by the roles or functions they serve in the network.

To learn more about the ArcFM UN data model and its required network categories, see the ArcFM UN Network Categories topic. To learn more about how to assign network categories, read the Esri help topic, Set or modify a network category assignment.

The following table displays the required network categories for the ArcFM XI series application, and in some cases, the specific tool.


ArcFM Editor XI

Network Category Application Tool

DistributionPipe

Editor

  • Isolation Trace (Gas)

Isolating

Editor

  • Isolation Trace (Gas & Water)

Meter

Editor

  • Isolation Trace (Gas & Water)

Regulator

Editor

  • Isolation Trace (Gas & Water)

ServicePipe

Editor

  • Isolation Trace (Gas)

Autoupdaters

Autoupdater Name Required Network Categories Details

Auto Angle Setter

None

N/A

Auto Structure Relate

None

Optionally, any category can be used for feature exclusion. To learn more, refer to the Auto Structure Relate topic.

DXI Integration - Create Vertex or Junction

None

N/A

Update Length

None

N/A

Update Line Terminal Connections

None

N/A

Valve Auto Size

None

Optionally, any category can be used for feature exclusion. To learn more, refer to the Valve Auto Size topic.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.