Delete Version On Session Completion

Administrators can configure an operational map to automatically delete a version and mark the associated session as complete once the version has successfully posted. Follow the steps below to set this up.

IMPORTANT: This functionality is only available to tenants that do not have Geodatabase Manager installed and configured along with Editor. Geodatabase Manager has a Delete Version Action Handler that can provide similar functionality.

  1. Select your operational map in Editor Maps.

    Editor Maps tab of the Editor plugin.

  2. Under Editor Settings, select your preferred option from the Delete Version On Session Completion drop-down.

    Editor Settings Delete Version On Session Completion drop-down options

    • Never means that versions are not deleted when the associated session has successfully completed.

    • Prompt means that in Editor XI, a user is prompted by a pop-up dialog asking them to confirm they want to delete the version when the associated session has successfully completed.

      Prompt that asks the user if they want to delete the version after the session is completed

    • Always means that versions are deleted after a session has successfully completed.

  3. Click Save in the Editor Settings section.

In addition to versions being deleted once a version has successfully posted, the associated session is also automatically marked complete. However, if a version encounters an issue that prevents it from successfully posting, the version is not deleted and the session is not marked complete.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.