Create Local Firewall Rule, Inbound Port 7443 to Portal for ArcGIS

Allow inbound port 7443 traffic to Portal for ArcGIS

After creating a local firewall rule to allow inbound port 6443 traffic to the ArcGIS Server, you need to create a local firewall rule to allow inbound port 7443 traffic to Portal for ArcGIS. Follow these steps:

  1. Open Windows Defender Firewall with Advanced Security.

    Refer to Microsoft’s support article for Firewall and network protection information.

  2. Right-click Inbound Rules and select New Rule.
  3. For Rule Type, select Port. Click Next.
  4. For Protocol and Ports, select TCP, then select Specific local ports and type 7443 in the field. Click Next.
  5. For Action, select Allow the connection. Click Next.
  6. For Profile, select when the rule should apply. Typically Domain is selected as most utilities are connected to a corporate domain, but select Private if you’re setting this up for a home network. Click Next.
  7. Type a descriptive name for the rule, an optional description, and click Finish.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.