Design Support for Sessions

Sessions with associated designs can be viewed in the Editor plugin for Solution Center.

To view the associated design information in Solution Center, click on the Design tab while viewing a session. The same information about the design displayed in Editor XI is visible in Solution Center, including indication of no associated design.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.