Shared Folder Install

If preferred, you can install ArcFM Editor XI by using a shared folder and the Add-In Manager within ArcGIS Pro.

  1. Launch ArcGIS Pro, if it’s not already running.
  2. Click Settings.
    ArcGIS Pro Settings button
  3. Select Add-In Manager.
  4. Select the Options tab.
    ArcGIS Pro Add-In Manager
  5. Select the Require Add-Ins to be digitally signed by a trusted publisher radio button.
  6. Click Add Folder and browse to the directory that contains the ArcFM Editor XI Add-In. Ensure you select the folder itself and not the add-in contained within the folder.
  7. Click OK.
  8. Reboot ArcGIS Pro to complete the installation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.