Update Line Terminal Connections

The out-of-the-box autoupdater, Update Line Terminal Connections, can be used within any domain network that has established terminal configurations. It maintains the terminal values on line features. The data within the FROMTERMINAL and TOTERMINAL fields are modified as necessary when edits are made to the network. When new devices or lines are added to the network, or existing features are moved or deleted, then connected lines are modified as necessary.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.