Optimal Install

Installing ArcFM Editor XI into ArcGIS Pro is as easy as double-clicking the add-in file.

  1. Close any open instances of ArcGIS Pro.
  2. Double-click the downloaded add-in. The file name should look like SE.Geospatial.ArcFM.AddIn-VersionNumber.esriAddinX.
  3. When prompted to install, click the Install Add-In button.
    Editor Add-In installation prompt
  4. Enjoy the satisfaction of a successful install!
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.