Rollout

You can ‘pin’ a version of Editor XI with the Rollout plugin in Solution Center. Administrators choose whether to update their editors with the latest patch build of a minor version of EXI, or choose a specific patch version for their editors to stay on. Rollout performs upgrades similar to the Rolling Updates feature in that it can’t perform downgrades if an editor manually installs a newer version of EXI.

In the case a digital copy of the download file is needed, Administrators can obtain a copy of the download link where the install files are uploaded.

For additional information on how to configure Rollout settings, see the Rollout topic in the ArcFM Solution Center Configuration Guide.

The View Release Notes button provides a link to the Editor XI myArcFM product space where a change log for the build and other news are available.

IMPORTANT: Rollout functionality specifically for EXI became available with version 11.1.0. Pinning to previous versions is unavailable.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.