Tracing Configuration for Named Traces

The Utility Network (UN) offers enhanced data fidelity, which allows for a fine-tuned understanding of your network and integrations with other sophisticated network analysis applications. But, with that comes data complexity for end users.

To ease the process of network tracing, Editor XI supports Named Traces. These are pre-configured traces that end users can simply call up and run, without setting barriers and without setting input and output parameters.

Configuring Named Traces is a two-step process:

  • In ArcGIS Pro, create the named trace configuration for the Utility Network.

  • In Solution Center > Editor > Editor Maps, point to the pre-saved trace configuration, and provide a user-friendly name.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.