Duct Attributes

This topic is linked to in an EXI error message. Duct Attributes must stay on this topic and it cannot be moved from the Configuration Guide without informing the EXI team of the change so code can be changed as well. This error message was created as part of their dev story EXI-3557.

When a domain is not properly set to a duct end field, the Conduit Manager Duct List tab displays a missing domain error message.

To fix this issue, the domains must be properly assigned to the fields in ArcGIS Pro. See Esri’s Assign Domain to Field help topic for details how to assign a domain.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.