Configure Send to Targets

Solution Center configuration allows you to set certain feature or non-spatial object class fields so they are automatically reset to the default or Null value each time the Target template is placed on the map. To learn more about Targets, refer to the Targets topic.

  1. To access this configuration, select your operational map from the drop-down on the Editor Maps tab in Solution Center.

  2. Then select the domain network containing the feature you want to configure from the Select a Domain Network to configure drop-down.

  3. Next, click on Send to Targets – Fields to Reset in the list under the drop-down.

  4. To the right of Send to Targets – Fields to Reset, select the Feature Class, Non-spatial Object, or Table you want to configure from the list.

  5. The Fields to Reset list updates to show the fields for the Feature Class, Non-spatial Object, or Table you selected. A check mark next to a field indicates that field is automatically reset to its default or Null value after the Target is placed on the map.

    Save to Target configuration showing field selections to reset when placed

  6. Click the box next to a field name to add or remove a check mark.

  7. Click the Save button to save your changes.

    ArcGIS Pro must be restarted for these changes to take effect.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.