Network Categories for Tracing

NOTE: For additional information regarding how to set network categories, see Esri’s help topic Set Network Category (Utility Network).

Tracing requires network categories must be applied to the desired ASSETTYPES so they participate in traces. Use the following table as a guide for required ASSETTYPES for various traces.

Network Categories

Domain Type

Description

E:Service Point

Electric

Applied to the meter ASSETTYPES that represent customers.

E:Switch

Electric

Applied to switch ASSETTYPES that can be used to operate the feature through Component Info.

E:Protective

Electric

Applied to protective device ASSETTYPES. Used by Component Info and by Editor XI’s protective device traces.

Isolating

Gas and Water

Applied to Controllable Valve ASSETTYPES that are operated to isolate sections of the network.

Meter

Gas and Water

Applied to the Meter ASSETTYPES that are impacted by the isolation trace.

Regulator

Gas and Water

Applied to the Regulator ASSETTYPES that are capable of isolating sections of the network.

DistributionPipe

Gas and Water

Applied to all Distribution Pipe ASSETTYPES that participate in the isolation trace.

ServicePipe

Gas and Water

Applied to all Service Pipe ASSETTYPES that are impacted by the isolation trace.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?