Select Your Service Domain Network

When an operational map (feature service) is successfully created, the Editor Maps tab displays similar to the image below.

You are prompted to select a Domain Network to configure. Select a domain network from the drop-down list. Then, click the button for your utility type (Electric, Gas, or Water). Currently, Editor XI does not yet support an operational map (feature service) with more than one utility network.

New operational map ready to select a domain network to configure

Once you have selected the utility type, different settings are presented for configuration specific to the utility type selected.

IMPORTANT: For your instance of Editor XI to properly work, you must have the below settings configured according to your service domain network type.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.