Internationalization / Localization

Editor XI supports being localized and only supports the language packs ArcGIS Pro can install. To install language packs and set them as your language of choice in ArcGIS Pro, see the available language options from Esri.

Currently, Editor XI supports the following languages for localization:

  • English

  • French

  • German

  • Portugese

If it is determined the translations of your language are not suitable, please contact Schneider Electric Technical Support.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.