Export the Asset Package

Administrators can review and modify the asset package data model and recreate the new file geodatabase as many times as needed until it meets the requirements and looks as expected. Read the Data Model Changes and Create a File Geodatabase for a Project for more detail. Once satisfied that the asset package represents your updated data model, you can use it with an enterprise geodatabase, store as a backup, and deploy it on another ArcGIS Pro instance and tenant. See Apply the Asset Package for more information.

To export your asset package:

  1. Open the Geoprocessing pane and search for the Export Asset Package tool.

  2. From the Catalog pane, Drag the Utility Network (UN) to the Input Utility Network field.

  3. Place a check by all Domain Networks as well as the Include data option.

    Export Asset Package options

  4. Review the export Folder Location and click Run. Make note of this exported file for future use. This is your exported asset package.

    NOTE: This tool can take 10–15 minutes to run.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.