Utility Network Configuration

Solution Center automatically installs the Editor XI plugin according to your licenses. However, your organization needs to complete additional configuration to properly work with your data.

To complete the necessary configuration, you need to start on the Editor Maps tab in Solution Center. Select an operational map from the drop-down list in green. To learn how to create an operational map, refer to Add a New Operational Map. The Editor Settings section is displayed.

To configure your domain network, select a service domain from the Select a Domain Network to configure drop-down. Depending upon the type of domain network, there is an opportunity to configure:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.