Configure Conduit Manager

Conduit Manager must be configured in Solution Center prior to using it in ArcFM Editor XI. Follow the steps below to configure Conduit Manager for your organization.
  1. On the Editor Maps tab in Solution Center for Editor, select your conduit Operational Map, then change the Select a Domain Network to configure drop-down to Structure.
    IMPORTANT: The Conduit Manager configuration appears in the drop-down only for Esri Utility Network version 4.0 and greater.

    The Structure vertical tabs display below the Select a Domain Network to configure drop-down.

  2. On the Structure Settings vertical tab, select the DuctDiameterUnits and MapUnits values that coincide with your organization mapping units from the appropriate drop-downs. In the MaxDucts field, type the maximum number of ducts you want a duct wall to contain (this limits the number of ducts created using the Create Duct Bank tool). Then click Save.

    IMPORTANT: If you have ducts in your map, changing the DuctDiameterUnit and MapUnit settings that your map was initially created with to a different unit of measure is not recommended or supported. Doing so could impact the spacing and size of ducts. It's recommended that once the unit of measure is set, you don't modify it.

  3. Select the Structure Field Names vertical tab, then set the field drop-downs as outlined in the table below. When you have set all the field values, click Save.

    Structure Field Name

    Field Name

    Description

    Available

    isavailable

    Applies to DuctEnd features in the StructureJunction class, as well as to Duct objects in the StructureEdgeObject table, to indicate that the corresponding duct is eligible to receive a new occupant.

    ConduitFacilityID

    assetid

    Identifier preferred by the customer implementing ArcFM, for conduit facilities.

    DuctBankGuid

    ductbankguid

    Maintained by ArcFM Conduit Manager.

    DuctDiameter

    diameter

    Floating point number that applies to Duct objects (StructureEdgeObject) and their corresponding DuctEnd features (StructureJunction). The length units associated with these values are specified by the DuctDiameterUnits configuration setting.

    DuctEndGuid

    ductendguid

    Maintained by ArcFM Conduit Manager.

    DuctEndShape

    ductcrosssectionshape

    Indicates the cross-sectional shape of the duct corresponding to a DuctEnd feature (StructureJunction).

    DuctFlagLabelText

    notes

    Maintained by ArcFM Conduit Manager.

    DuctFlagOutlineId

    ductflagoutlineid

    Maintained by ArcFM Conduit Manager.

    DuctFlagRotation

    ductflagrotation

    Maintained by ArcFM Conduit Manager.

    DuctFlagScale

    ductflagscale

    Maintained by ArcFM Conduit Manager.

    DuctID

    ductid

    User-assignable identifier for a duct with a bank. Found on both the Duct (StructureEdgeObject) and its associated DuctEnd features (StructureJunction)

    DuctOccupantDescription

    occupantdescription

    Maintained by ArcFM Conduit Manager.

    LeaderLineAttachPoint

    leaderlineattachmentpoint

    Maintained by ArcFM Conduit Manager.

    Material

    material

    NumberOfAvailableDucts

    numavailableducts

    Maintained by ArcFM Conduit Manager.

    Occupied

    isoccupied

    (True/False) Indicates whether a duct is occupied. Automatically initialized by ArcFMConduit Manager while ducts are being edited, but user can assign an overriding value. Found on both the Duct (StructureEdgeObject) and its associated DuctEnd features (StructureJunction).

    StructureAddress

    name

    Address of the structure.

    StructureFacilityID

    assetid

    Structure identifier preferred by the customer implementing ArcFM.

    WallHeight

    wallheight

    The height of the structure wall.

  4. Assign the required Network Categories outlined in the Conduit Manager Network Categories topic.
At this point Conduit Manager is configured and you can start using it in ArcFM Editor XI.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.