ArcGIS Server Configuration

This section covers all the necessary configuration that takes place in ArcGIS Server Manager for Server Object Interceptors.

IMPORTANT: The ArcFM Autoupdater XI SOI does not currently support geometry modifications in a different spatial reference than the source. Consequently, any map with the SOI enabled on its source should not be projected in a different spatial reference than the source.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.