Verify Install and Check Build Number

To verify that ArcFMEditor XI was successfully installed, or to check the ArcFM Editor XI build number, follow these steps:

  1. Launch ArcGIS Pro, if it’s not currently running.
  2. Click Settings.

    ArcGIS Pro Settings button

  3. On the left side of the window, locate ArcFM Editor XI.
  4. View the version installed on your system, which verifies the installation was successful.

    ArcFM Editor XI version

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.