Install and Configure Solution Center

To properly configure Editor XI, most of the configuration has to be completed in Solution Center within the Editor plugin. Thus, it is important to install and verify access early in the implementation process.

Go to the myArcFM article ArcFM Solution Center to find out more about the application and to download the installer.

NOTE: Solution Center has its own configuration guide! See ArcFMSolution Center – Implementation Guide for more information.

This section covers all the possible Editor XI configuration within Solution Center; however, not all settings are required to complete your installation of Editor XI.

Utility network operational map configuration is necessary for your EXI implementation to work properly.

We’ll walk through each of the tabs within the Editor plugin. Once you have completed configuration in Solution Center, continue on to the next step of this guide to install Editor XI.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.