Delete Version on Session Completion

Administrators can configure Session Manager to delete versions associated with completed sessions. If configured, Session Manager marks a session as complete, and deletes the associated version once that session version has posted successfully. This is configured on the operational map. Refer to the Delete Version on Session Completion topic under Editor Maps to learn more.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.