Workflow Families

Each subtab on the Default Workflow Studio tab and the Studio tab represents a type of workflow family that corresponds to where the workflows are executed (hosted versus specific client applications, such as Editor, Designer XI, etc.). On the Default Workflow Studio tab, out-of-the-box workflows are provided for each workflow family type. While workflow families have much in common, some have some important distinctions.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.