Rolling Updates

Editor XI has the power to update through Solution Center. This allows Schneider Electric to seamlessly update the application with the latest release without taking time from administrators to install these new versions on their Editor machines. Users are notified when an updated version is available when they log in to EXI and are requested to manually restart their session of ArcGIS Pro to install and accept the updates. These updates include major, minor, and patch releases that have been announced on myArcFM.

Rolling updates continues to look for the latest version of EXI unless a version has been pinned in Solution Center.

Rolling Updates does not support a downgrade scenario. If a downgrade is needed, submit a ticket to Schneider Electric support.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.