Deploy the Autoupdater XI Extension

Since the Autoupdater XI SOI is an extension for ArcGIS Server, the extension must be deployed following Esri’s instructions. Refer to Esri’s Deploy an extension article.

To download the necessary file, visit the myArcFM website, and click on the Login button in the upper right corner. Log in using your customer credentials. Navigate to Support > Product Downloads. There are tabs across the center of the page with different product names. Select the ArcFM Editor XI tab. Click on ArcFM_Autoupdater_XI to download the file called ArcFM_Updater_XI.soe.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.