Map Layer Requirements
There are some map layer requirements for your map to work properly. The items below outline those requirements.
Integrated Product Configurations
If you have an integrated Editor XI and Designer XI configuration, it is required that they share an operational map. This integration is visible within Solution Center. On the Mapping plugin, select the Operational Maps tab, then select your operational map in the left pane. In the right pane, in the Overview tab, you see your configured ArcFM XI products toggled on in green. If you have both Editor XI and Designer XI toggled on, you must share an operational map.
Using Layers From Different Operational Maps
Subtype Group Layers
Subtype group layers are required in Editor XI in order for some functions to work properly. If there are feature classes in your map that are missing subtype group layers, the following error message appears in Esri’s notification doc pane:
Any layers listed in the notification are not included in a subtype group layer and need to be set up within one.
For additional information about adding group layers to your map, see Esri’s Draw Preset layers documentation. For information on how to add subtype group layers to your map, see Esri’s Subtype group layers and tables documentation.