ArcGIS Pro Configuration

Configuring utility GIS data for use within ArcGIS Pro requires creation of the Utility Network (UN). The UN provides the network topology rules that act as the foundation for the domain (electric, gas, water) network.

To build the UN, we provide two downloadable asset packages for the electric domain to get you started. These asset packages are a type of file geodatabase that models the schema, properties, related layers, related tables, and data of a UN. It contains the definitions and parameters of the ArcFM Editor XI Data Model that enable a transition between databases for data design, loading, and rollout.

This data model contains sample data and aligns with UN requirements as follows:

  • Feature layers are modeled based on UN asset groups and asset types.

  • Assets contained in the equipment hierarchies that are children of feature layers are modeled in related tables.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.