Administrating Service Configurations

To delete an operational map configuration from the tenant, navigate to the Mapping plugin on the home screen of Solution Center.

Mapping plugin

On the Operational Maps tab, locate the operational map you want to delete from the list and select it.

Above the Delete button in the pane on the right side, notice the warning message. Deleting an operational map can cause adverse effects. For that reason, the app prompts you to confirm delete once you click the Delete button.

IMPORTANT: Operational maps with sessions still in an open state can’t be deleted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.